Skip to main content
Graduate
April 19, 2022
Question

Not able to connect to Sensor tile Box

  • April 19, 2022
  • 2 replies
  • 1190 views

Hello,

I have recently purchased Sensortile BOX , i can connect to it using st ble sensor application and it has a default cloud logging application.

I want to flash other applications like blemlc , etc ut not ale to connect to it

Attached are the pictures of the connection and issue.

Is it possible to flash other images over FOTA?

please assist!

Br,

0693W00000LyH02QAF.png 

0693W00000LyH07QAF.jpg 

0693W00000LyH0bQAF.jpg

    This topic has been closed for replies.

    2 replies

    ST Employee
    April 22, 2022

    Hi @darla14​ ,

    Yes, it should be possible.

    Did you try to erase the MCU memory and try to flash the code in JTAG (programming) mode or DFU mode? Here an explanation about how to do it --> LINK

    -Eleon

    darla14Author
    Graduate
    April 22, 2022

    Hello @Eleon BORLINI​  ,

    Yes I tried erasing but the problem is "No STM32 Target found". I tried all the options of drop down ( USB, JTAG, DFU....)

    Could be some issue with my connections or faulty cable.

    I was just wondering cant I flash over the air?Any such binary or mode?

    Rgds,

    Visitor II
    July 7, 2022

    I had a similiar issue with the Sensortile Devkit. Did you try holding the reset button while pressing connect while on the SWD connection? The reset mode should be hardware reset as shown in your image. May be this helps. :)

    darla14Author
    Graduate
    July 13, 2022

    Thanks @SThek.1​  , i will try this