Skip to main content
Visitor II
September 19, 2024
Question

Obsolescence of IIS328DQTR and equivalent components

  • September 19, 2024
  • 1 reply
  • 693 views

Hey! 

If I well understood the component IIS328DQTR will be at least "NRND" in 2025. 

The IIS3DHHC seems to be a good substitute but it doesn't have all the interrupt features of the IIS328DQTR. 

Can you confirm the lifetime of the IIS328DQTR? 

Do you have a 3-axis digital accelerometer with the feature: "The device may be configured to generate an interrupt signal through inertial wakeup events, or by the position of the device itself."

Kind regards

Charles D

 

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    September 20, 2024

    Hi @CharlesD_4_ElsysDesign ,

    from 2025 the commitment ends and thereafter its availability will depend on market conditions. However, we recommend for new designs to consider newer generation products such as IIS2DLPC