Only getting 0's from LSM303AGR accelerometer.
Hi,
I've got a STEVAL-MKI173V1 board hooked up to my uC. I ported over the driver from:
https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lsm303agr_STdC
I'm able to read valid magnetometer values but almost always get 0's from the accelerometer.
Here is the code:
uint8_t whoamI, rst;
int pDataM[3];
int pDataA[3];
int16_t pDataARaw[3];
int16_t pDataMRaw[3];
float acceleration_mg[3];
float magnetic_mG[3];
uint32_t ret;
whoamI = 0;
ret = lsm303agr_xl_device_id_get(COMPASS_ACCL_ADDR, &whoamI);
//if ( whoamI != LSM303AGR_ID_XL )
// while (1); /*manage here device not found */
whoamI = 0;
ret = lsm303agr_mag_device_id_get(COMPASS_MAG_ADDR, &whoamI);
//if ( whoamI != LSM303AGR_ID_MG )
//while (1); /*manage here device not found */
ret = lsm303agr_mag_reset_set(COMPASS_MAG_ADDR, PROPERTY_ENABLE);
do {
lsm303agr_mag_reset_get(COMPASS_MAG_ADDR, &rst);
} while (rst);
ret = lsm303agr_xl_block_data_update_set(COMPASS_ACCL_ADDR, PROPERTY_ENABLE);
ret = lsm303agr_mag_block_data_update_set(COMPASS_MAG_ADDR, PROPERTY_ENABLE);
/* Set Output Data Rate */
ret = lsm303agr_xl_data_rate_set(COMPASS_ACCL_ADDR, LSM303AGR_XL_ODR_1Hz);
ret = lsm303agr_mag_data_rate_set(COMPASS_MAG_ADDR, LSM303AGR_MG_ODR_10Hz);
ret = lsm303agr_xl_full_scale_set(COMPASS_ACCL_ADDR, LSM303AGR_2g);
lsm303agr_mag_set_rst_mode_set(COMPASS_MAG_ADDR,
LSM303AGR_SENS_OFF_CANC_EVERY_ODR);
/* Enable temperature compensation on mag sensor */
ret = lsm303agr_mag_offset_temp_comp_set(COMPASS_MAG_ADDR, PROPERTY_ENABLE);
/* Enable temperature sensor */
lsm303agr_temperature_meas_set(COMPASS_ACCL_ADDR, LSM303AGR_TEMP_ENABLE);
lsm303agr_xl_operating_mode_set(COMPASS_ACCL_ADDR, LSM303AGR_HR_12bit);
/* Set magnetometer in continuous mode */
ret = lsm303agr_mag_operating_mode_set(COMPASS_MAG_ADDR,
LSM303AGR_CONTINUOUS_MODE);
USTIMER_Delay(200 * MILLI_SEC);
//val = 0;
lsm303agr_xl_status_get(COMPASS_ACCL_ADDR,®.status_reg_a );
printf("reg.status_reg_a.zyxda: %x\n\n\n", reg.status_reg_a.zyxda);
memset(pDataARaw, 0x00, 3 * sizeof(int16_t));
ret = lsm303agr_acceleration_raw_get(COMPASS_ACCL_ADDR,
pDataARaw);
acceleration_mg[0] = lsm303agr_from_fs_2g_hr_to_mg(
pDataARaw[0]);
acceleration_mg[1] = lsm303agr_from_fs_2g_hr_to_mg(
pDataARaw[1]);
acceleration_mg[2] = lsm303agr_from_fs_2g_hr_to_mg(
pDataARaw[2]);
printf("Acceleration raw:%d %d %d\r\n",
pDataARaw[0], pDataARaw[1], pDataARaw[2]);
printf("Acceleration [mg]:%4.2f %4.2f %4.2f\r\n",
acceleration_mg[0], acceleration_mg[1], acceleration_mg[2]);
ret = lsm303agr_mag_status_get(COMPASS_MAG_ADDR, ®.status_reg_m);
memset(pDataMRaw, 0x00, 3 * sizeof(int16_t));
ret = lsm303agr_magnetic_raw_get(COMPASS_MAG_ADDR, pDataMRaw);
magnetic_mG[0] = lsm303agr_from_lsb_to_mgauss(
pDataMRaw[0]);
magnetic_mG[1] = lsm303agr_from_lsb_to_mgauss(
pDataMRaw[1]);
magnetic_mG[2] = lsm303agr_from_lsb_to_mgauss(
pDataMRaw[2]);
printf("Magnetic field [mG]:%4.2f %4.2f %4.2f\r\n",
magnetic_mG[0], magnetic_mG[1], magnetic_mG[2]);
heading = getHeading(magnetic_mG[X], magnetic_mG[Y]);
printf("heading: %f\n", heading);The results are as follows (sitting on my desk):
$ c2
reg.status_reg_a.zyxda: 1
Acceleration raw:0 0 0
Acceleration [mg]:0.00 0.00 0.00
Magnetic field [mG]:39.00 -31.50 -202.50
Mag[Y]: -31, May[X]: 39
heading: 321.519806
$ c2
reg.status_reg_a.zyxda: 1
Acceleration raw:0 0 0
Acceleration [mg]:0.00 0.00 0.00
Magnetic field [mG]:34.50 -31.50 -195.00
Mag[Y]: -31, May[X]: 34
heading: 317.642548I need to do pitch and roll correction for the compass.
Any ideas as to what I'm doing wrong?
Thanks,
-Steve