Skip to main content
Visitor II
April 16, 2021
Question

P-NUCLEO-IKA02A1 EVK

  • April 16, 2021
  • 3 replies
  • 1252 views

Hi Sir/Mdm,

I tested the EVK with the lowest PPM in clean air was 6ppm yesterday and today I tested again in clean air was 2.4ppm and is fluctuating. When I first got this EVK, it was 0.6ppm which < 1, after testing a few rounds with CO gas, then I won't drop to that point. Appreciate if you could give us some support on this problem, thanks.

    This topic has been closed for replies.

    3 replies

    ST Employee
    April 16, 2021

    Hi @jason239955_st​ ,

    I'm not an expert of gas sensor, since it is not from ST but from this other company, Figaro (TGS5141-P00).

    I see from the datasheet (that you can also find in attachment to this post) that there could be up to ±10ppm equivalent offset, but I don't know whether it can fluctuate...

    As a standard procedure we suggest for our environmental sensors, I would suggest you to run a 85°C bake, to clean any post-solder effect.

    My first suggestion is however to directly contact Figaro for an effective help.

    Let me then know if you can find out more from their side.

    -Eleon

    Visitor II
    April 16, 2021

    Hi Eleon,

    I am using this evaluation board with the Nucleo-L053R8 to do the evaluation and getting the result of the CO sensor.

    After testing a few rounds, I noticed there was a setting "T" on the for test the sensor using the NUCLEO together with the sensor expansion board. 

    I keep getting error while try to run the test procedure, screenshot attached

    Datasheet not mention the test procedure, I am confused with the error message "JP2 pin 1 was not connected" what does that mean? and what should I do?

    JP2 on the sensor expansion board is GAIN settings, I tried shorted pin 1-2, same error, and tried shorted 2-3 also same error. Appreciate if you could help on this issue.

    ST Employee
    April 20, 2021

    Hi @jason239955_st​ ,

    Are you using the board with the default firmware uploaded?

    As another interface channel, as shown in the UM2247 user manual, p.11, you could use also Unicleo-GUI to interface the board. It contains a Custom Fields window which fully supports the P-NUCLEO-IKA02A1 expansion board to show the measured values in a graph. The source code for NUCLEO-L053R8, NUCLEO-F401RE and NUCLEO-L476RG boards is available in the X-CUBE-IKA02A1 software package as DataLogCustomLite sample.

    Did you already tried this solution?

    -Eleon