Please provide guidance on VL53L3 calibration.
The "VL53LX API Specification" 1.1.4.2352 lists 13 "calibration functions" but provides little guidance on what they do and when they should be called. The VL53L3 data sheet says calibration is required and "The detailed procedure is provided in the device driver user manual" - but I do not see such a user manual (is it the "VL53LX API Specification", or something different?). The example application does not perform calibration.
Is there any guidance on the use of these functions to optimise performance of the VL53L3? What about sample code that shows them in use?