Possible to connect VL53L1X to sensor hub on LSM6DSL or LSM6DSR?
The LSM6DSL, LSM6DSR have a sensor hub and I'd like to connect the VL53L1X Time of flight sensor to the sensor hub and have the IMU automatically read information from the VL53L1X.
From reading the sensor hub documentation in the datasheets as well as AN5192, it seems there is only one write data register and the sensor hub only has subaddress and register for the transfer but the VL53L1X needs multiple bytes to do the read.
Thanks.