Skip to main content
Visitor II
August 20, 2014
Question

Possible to reset interrupt when LIS3DH is disabled, or other possibililty?

  • August 20, 2014
  • 2 replies
  • 821 views
Posted on August 20, 2014 at 03:35

Hi,

I have the LIS3DH setup to trigger interrupt 1 when '6 direction movement recognition' on all axis using HP filter example on application note page 24.

This works well.

After being set I read the HP_FILTER_RESET and also the INT1_SRC which resets the filter position and clears the interrupt, ready to sense movement again.

If I disable the LIS3DH with 0x00 in ctrl_reg1 while the interrupt is triggered, the interrupt stays triggered (it is active low, so it stays low). If I read the HP_FILTER_RESET and also the INT1_SRC the interrupt does not reset.

(1) Is there any way to clear the interrupt like I can do when the LIS3DH is 'enabled'?

(2) My goal is to reset the interrupt (to high state since it is active low) after it has been triggered and disable it  even if the device is still moving. Is this possible?

(3) Is there a command that will drive the interrupt line high directly regardless of movement?

Thank you

#lis3dh-interrupt
    This topic has been closed for replies.

    2 replies

    dtrouttAuthor
    Visitor II
    September 24, 2014
    Posted on September 24, 2014 at 02:39

    For anyone interested I received this comment from ST support which satisfies my need...

    ''

    the best way would be to disable I1_AOI1 before going to power down. That will guarantee that the interrupt is de-asserted before going to power down.''

    Visitor II
    December 9, 2015
    Posted on December 09, 2015 at 16:39

     Dan,

       What was the actual address of the HP_FILTER_RESET for the LIS3DH?

    Sorry to jump on this so late... your post is the only place on the entire internet that mentions this register other than the POS datasheet.