Powering LIS2DS12 sensor with 2.5 volts
by some mistake, we have a large batch of boards with LIS2DS12 sensor and STM32G030F6P6 mcu powered with 3.3 volts.
but the maximum voltage for LIS2DS12 is 2.0 volts, and absolute minimum voltage for STM32G030F6P6 is 2.0 volts. so we tried to adjust on board power regulator down to 2.0 volt but we had boot problems with the mcu.
so the question is 2.2 volt the absolute maximum of LIS2DS12 is safe for long term working condisitons ? because STM32G0 looks fine with 2.2 volts.
also can we run LIS2DS12 with 2.5 volts (0.3 volts over the absolute maximum) i am asking this because we have a test batch and LIS2DS12 chips are working fine with 3.3 volts over weeks without single fault.