Problem with Bluecoin and echo cancellation
Hy,
I'm trying to do some tests on echo suppression using evaluation boards BlueCoin and CoinStation.
The software I use is the one provided by ST to interact with BlueCoin that is, FP-"AUD-SMARTMIC1 GUI.exe" in addition to the
audacity.exe program.
As specified in the document , "Getting started with STM32Cube function pack for MEMS microphones acquisition, advanced audio
processing and audio output" (UM2219) paragraph 4.5, I would expect to hear on the output left only the signal picked up by
the microphone while on the right output the microphone signal plus the audio fragment.
I actually hear the microphone signal plus the audio fragment on both output left and right.
What should I do to hear on the output left only the microphone (and then have the proof that the echo cancellation worked) ?
The program loaded on the board BlueCoin is the version 1.0.0 ( Device presentation string: OSX SMARTMIC1 | BlueCoin Dev Kit |Embedded Microphones|1.0.0)
Thank you