Skip to main content
Visitor II
July 24, 2020
Question

Problem with setup of HS sensor DataLog application for STWINKT1

  • July 24, 2020
  • 2 replies
  • 870 views

Hello everyone, i'm a beginner,

I recently bought a STWINKT1. I'm trying to setup the HSDataLog, using the: '' quick start guide HS sensor dataLog application for STWINKT1. Running USB_DataLog_Run.bat the results is: no devices. I installed STM32CubeProgrammer, and the software correctly work. Do you have any suggestions?

Thanks

    This topic has been closed for replies.

    2 replies

    ST Employee
    August 27, 2020

    Hi @RMess.1​ , sorry for the late feedback mostly due to vacation time... if I well understand your problem, you run USB_DataLog_Run.bat but it is not able to detect you, right? Did you configured the related VCOM port in the correct way (as shown in the below picture)?

    0693W000002lWpDQAU.png

    I also suggest you to give a look at this article, which may help you to deal with the Example – HS_DataLog --> http://www.emcu.eu/mems-predictive-maintenance-using-an-intelligent-logging-kit-for-iot-applications/

    Regards

    ST Employee
    September 9, 2020

    Hi @RMess.1​ ,

    please check this other thread if it can be of some help.

    -Eleon