Skip to main content
Visitor II
February 10, 2024
Question

Problem with Unicleo GUI

  • February 10, 2024
  • 2 replies
  • 1114 views

Hello . 

I have to boards L476RG and 303RE and of course IKS01A3 . 

After installing Unicleo , I can't connect to that IKS (It's not even showing port )  . I'm changing boards but still It can't see it . 

On some tutorials some lady was coping some files to the folder which is being created after connecting the board to USB . But my board is not even existing in examples . 

Simple question : How I can connect IKS using my boards (476RG or 303RE ) vand see the values from sensors ? 

Best Regards , 

Samu

 

 

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    February 13, 2024

    Hi @pepebisup12 ,

    Welcome to ST Community!

    Unfortunately, this combination of boards X-NUCLEO-IKS01A3 + NUCLEO-L476RG (and NUCLEO-F303RE) is no more supported in the X-CUBE-MEMS1 package. You could manually port DatalogExtended firmware from X-CUBE-MEMS1 to your board.

    Visitor II
    February 16, 2024

    Thank you for your reply. 

    I have found it in x-Nucleo-iks01a3_quick_start_guide

    pepebisup12_0-1708058319423.png

    However, I have checked the latest supported boards in MEMS1 library folders  and they are :

    NUCLEO-F401RE
    NUCLEO-L073RZ

    NUCLEO-L152RE

    NUCLEO-U575ZI-Q

     

    Can you confirm this?

    Best Regards, 

    Pepe

    Technical Moderator
    March 5, 2024

    Hi @pepebisup12 ,

    Yes, the boards you are loooking are not supported by X-CUBE-MEMS1. NUCLEO-L476RG used to be supported, that is why it is mentioned in the getting started document for X-NUCLEO-IKS01A3 but it is not supported anymore.