Problems with temperature affecting the readings from LSM6DS3TR.
I'm developing a product using the LSM6DS3TR. As per the data sheet the data from the device should not be influenced by temperature more than 1.5% between -40 and +85 degrees. I see wild swings in the data for the Y-Axis Accelerometer when the temperature changes. I can actually just breath on the device and see the data skew. When placed in the sun the data really swings, but only for the Y-Axis. Any help would be greatly appreciated. Rob