Programming the sensor tile
Good day,
I have purchased a sensor-tile and would like to code said tile. The board is receiving power and the SWD connections are correct and double checked. Then when the st link is plugged in and one wants to debug and program the micro an error states that the target is not detected. Therefore I cannot code the micro. These are the only connections to and from the micro. I am using a ST-Link V2 to program this product. Also when the board has power I cannot pick it up through Bluetooth. Any help will be greatly appreciated.