Skip to main content
Visitor II
May 9, 2016
Question

q.lsm6ds3 anti-aliasing filter order

  • May 9, 2016
  • 2 replies
  • 911 views
Posted on May 09, 2016 at 13:05

hi,

I've got a few questions.

1. what is the order anti-aliasing filter of the Acc?

2. what is the order anti-aliasing filter of the Gyro?

3. how does the DLPF1 filter help me if the cut-off freq is higher then nyquist freq?

thank you,

amir

#lsm6ds3 #lsm6ds3
    This topic has been closed for replies.

    2 replies

    Visitor II
    June 24, 2016
    Posted on June 24, 2016 at 11:19

    Hi all,

    I have similar questions regarding the LSM9DS1:

    1. The Acceleration ODR choices go down to 10 Hz, however the bandwidth selection, presumable an anti-aliasing filter, is limited to 50Hz. Thus, when sampling at 10Hz or 50Hz with a bandwidth selection of 50Hz severe aliasing is to be expected. Is there a way to avoid this?

    2. The accelerometed digital filter operation is not documented properly. What dow ''high resolution'' refer to? How is LPF or HPF selected?

    ST Employee
    June 30, 2016
    Posted on June 30, 2016 at 14:07

    Hi Amir,

    please refer to the Chapters 2.6 and 2.7 of the AN4650 Application Note downloadable from ST web pages:

    http://www.st.com/resource/en/application_note/dm00157511.pdf

    Thank you and best regards,

    Petr

    Visitor II
    February 8, 2017
    Posted on February 08, 2017 at 00:48

    I don't see those chapters in AN4650, or anything that answers the questions: what is the order of the antialias filters. I have another question: what is the cutoff frequency and order of the gyro antialias filter?

    Dan