Skip to main content
Visitor II
October 23, 2015
Question

Query regarding IMU sensor for Golf Swing Analyses

  • October 23, 2015
  • 3 replies
  • 1206 views
Posted on October 23, 2015 at 08:33

I am in search of 6 or 9 axis IMU mems sensor for golf swing analyses device.

The device would be somewhat like  http://3bayslife.com/zone-1/ 

Should I go for 6 axis DOF or 9 axis DOF? Low power operation is must. 

Also the captured data is to be transmitted via bluetooth to smartphone. 

Suggest me with suitable options for 6 or 9 axis MEMs (which one is better and why?) and also the bluetooth socs that are suitable for this project.

#golf-swing-analyses
    This topic has been closed for replies.

    3 replies

    rahul23Author
    Visitor II
    October 29, 2015
    Posted on October 29, 2015 at 08:56

    Unfortunately, I do not see any replies coming. 

    This is my first post on ST community. 

    Visitor II
    October 29, 2015
    Posted on October 29, 2015 at 09:53

    Unfortunately, this forum is not very useful. Perhaps you should try invensense or bosch.

    Visitor II
    March 26, 2024

    I also need a device to analyze the golf swing so I can video it and put it on YouTube. Where can I get this device?