Question
Question about rtnRate
Posted on July 10, 2016 at 20:53Hi I would like to get the signal strength very much.So, please let me ask two questions.The first one is about a function in vl6180x_api.c.julien@ST said like following in the Discussion Board named ''How to measure the ToF'':>No, there is no way to access to the time of flight. Only distance, signal strength, ambiance rate ...>Signal strength is the amount of the photons coming back from the target.>You can access to this field ''rtnRate'' in the struct ''VL6180x_RangeData_t'' below.So, I saw the _GetRateResult function in the vl6180x_api.c.However, I couldn't understand clearly following part:> calcConvTime = m_refConvTime;> if (m_rtnConvTime > m_refConvTime) {> calcConvTime = m_rtnConvTime;> }> if (calcConvTime == 0)> calcConvTime = 63000;Please tell me what this function does here.Next, is the value of the register named RESULT__RANGE_RETURN_RATE the same to that of rtnRate referred to by julien@ST?If they have the same value, can I get the signal strength with accessing this register directly? Alternatively, can we get the range_return_rate as the signal strength with decoding it in 9.2 format (devides the value by 128)?>We encourage our customers to use the API, no register access, available in ST.COMBy the way, how can I access the signal strength without using api?Because we couldn't transport api functions completely, we would like to create an original function to get the value. Can't we do that?Best regardsIshikawa #vl6180x