Question
Question about X-NUCLEO-IKS01A1.
Posted on July 18, 2016 at 16:01
I have an X-NUCLEO-IKS01A1 board. There is a LSM6DS0 on the board but the following functions
DrvStatusTypeDef BSP_ACCELERO_Enable_Free_Fall_Detection_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Disable_Free_Fall_Detection_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Get_Free_Fall_Detection_Status_Ext( void *handle, uint8_t *status );
DrvStatusTypeDef BSP_ACCELERO_Set_Free_Fall_Threshold_Ext( void *handle, LSM6DS3_ACC_GYRO_FF_THS_t thr );
DrvStatusTypeDef BSP_ACCELERO_Enable_Pedometer_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Disable_Pedometer_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Get_Pedometer_Status_Ext( void *handle, uint8_t *status );
DrvStatusTypeDef BSP_ACCELERO_Get_Step_Count_Ext( void *handle, uint16_t *step_count );
DrvStatusTypeDef BSP_ACCELERO_Reset_Step_Counter_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Set_Pedometer_Threshold_Ext( void *handle, uint8_t thr );
DrvStatusTypeDef BSP_ACCELERO_Enable_Tilt_Detection_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Disable_Tilt_Detection_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Get_Tilt_Detection_Status_Ext( void *handle, uint8_t *status );
DrvStatusTypeDef BSP_ACCELERO_Enable_Wake_Up_Detection_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Disable_Wake_Up_Detection_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Get_Wake_Up_Detection_Status_Ext( void *handle, uint8_t *status );
DrvStatusTypeDef BSP_ACCELERO_Set_Wake_Up_Threshold_Ext( void *handle, uint8_t thr );
DrvStatusTypeDef BSP_ACCELERO_Enable_Single_Tap_Detection_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Disable_Single_Tap_Detection_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Get_Single_Tap_Detection_Status_Ext( void *handle, uint8_t *status );
DrvStatusTypeDef BSP_ACCELERO_Enable_Double_Tap_Detection_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Disable_Double_Tap_Detection_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Get_Double_Tap_Detection_Status_Ext( void *handle, uint8_t *status );
DrvStatusTypeDef BSP_ACCELERO_Set_Tap_Threshold_Ext( void *handle, uint8_t thr );
DrvStatusTypeDef BSP_ACCELERO_Set_Tap_Shock_Time_Ext( void *handle, uint8_t time );
DrvStatusTypeDef BSP_ACCELERO_Set_Tap_Quiet_Time_Ext( void *handle, uint8_t time );
DrvStatusTypeDef BSP_ACCELERO_Set_Tap_Duration_Time_Ext( void *handle, uint8_t time );
DrvStatusTypeDef BSP_ACCELERO_Enable_6D_Orientation_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Disable_6D_Orientation_Ext( void *handle );
DrvStatusTypeDef BSP_ACCELERO_Get_6D_Orientation_Status_Ext( void *handle, uint8_t *status );
DrvStatusTypeDef BSP_ACCELERO_Get_6D_Orientation_XL_Ext( void *handle, uint8_t *xl );
DrvStatusTypeDef BSP_ACCELERO_Get_6D_Orientation_XH_Ext( void *handle, uint8_t *xh );
DrvStatusTypeDef BSP_ACCELERO_Get_6D_Orientation_YL_Ext( void *handle, uint8_t *yl );
DrvStatusTypeDef BSP_ACCELERO_Get_6D_Orientation_YH_Ext( void *handle, uint8_t *yh );
DrvStatusTypeDef BSP_ACCELERO_Get_6D_Orientation_ZL_Ext( void *handle, uint8_t *zl );
DrvStatusTypeDef BSP_ACCELERO_Get_6D_Orientation_ZH_Ext( void *handle, uint8_t *zh );
Implemented ONLY for LSM6DS3 – for the chip that UNAVAILABLE on the board.
Well…some time ago I’d have been furious but today I’ve even not surprised.
Any way - to add the same functionality for
LSM6DS0 that IS ON BOARD – should I just change registers or it would be some change in algorithm?