Skip to main content
Visitor II
November 17, 2017
Question

Read\Write LIS2DH12 with I2C using DMA

  • November 17, 2017
  • 1 reply
  • 736 views
Posted on November 17, 2017 at 15:13

Hi, I am trying to read the LIS2DH12 using the I2C and DMA.

I got everything configured via STM32CubeMx. 

When I want to read the LIS2DH12 (WHO_AM_I @0x0F) I call:

HAL_I2C_Master_Receive_DMA(&hi2c1, (uint16_t)SLAVE_ADDRESS, (uint8_t *)I2CRxBuf, 1);

I have defined the below:

 SLAVE_ADDRESS 0x330F   // (slave address 0x33 and read adress 0x0F

char I2CRxBuf[5];

I wait for it to complete the receive first:

while (HAL_I2C_GetState(&hi2c1) != HAL_I2C_STATE_READY);

Then print the value on the screen. It always stay zero.

What am I doing wrong?

    This topic has been closed for replies.

    1 reply

    Visitor II
    April 19, 2018
    Posted on April 19, 2018 at 16:33

    I am facing same problem.

    Have you solved this problem?