Reading HALL Sensors values from HALL interface
Hi dear members,
I am trying to understand complete how to drive bldc motor.And I would like to use hall interface in stm32.how can I manage to read commutation using hall sensors which registers I couldn't find it in reference manuel.And also how can I configure prescaler if motor is low speed because datasheet say "Program the time base: write the TIMx_ARR to the max value (the counter must be cleared by the TI1 change. Set the prescaler to get a maximum counter period longer than the time between 2 changes on the sensors" set the prescaler is hard like that