Skip to main content
Graduate II
September 14, 2024
Question

Reset SFLP on LSM6DSV16?

  • September 14, 2024
  • 1 reply
  • 1170 views

HI,

Is there any way to reset SFLP "Game vector" readings at runtime, once SFLP enabled?

For instance, after few minutes of SFLP run, it reports (after quaternion to Euler conversion) YAW: 1.5, PITCH: 0.5, ROLL: 0.1. And I'd like to reset Yaw to 0 (zero). Is there any way to do so on chip (manipulating offsets, "soft" algorithm reset etc.)?

Surely it is possible to use external matrix to compensate for the above in software but maybe there is some "undocumented" way to ask SFLP to do the same?

 

Thanks

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    November 13, 2024

    Hi @bear2023R ,

    Unfortunately, it is not possible to do this.