schizophrenic LIS3DS0
Hi everybody,
We are using LIS3DS0 on the ISK01A1 board monted on a Nucleo F103-RB...Our software is based on HAL drivers (got in the cube).We met this strange issue in some of our boards (we confirmed the test with many students and dozens of boards):1- we plug the board2- the accelerometer failed to initialize. (due to the WHO_AM_I register which is 0xD4 instead of 0x68).We can reset again and again our STM32, without any change.Then we program a flush of registers of the LIS3DS0.We confirm the registers seems to correspond to another component (L3G3200D) !(WHO_AM_I of 0xD4, )But, when we do the following steps, the component run well :1- plug the board2- -> fail to initialize3- get off the JP2 jumper4- ensure temporarly 0V on the Vcc of sensor (with wire) (to avoid a 2V power by I2C bus)5- get on the JP2 jumper-> It works!We can reset our STM32, it works each time.Any idea????!!!Thanks! #lis3ds0-iks01a1-initialize-fail