Skip to main content
ST Employee
September 30, 2019
Question

SensorTile.box #4: A compass and a level in your pocket can always be useful

  • September 30, 2019
  • 1 reply
  • 696 views

While the Barometer application involves basically all the environmental sensors on the SensorTile.box, the Compass&Inclinometer application is almost uniquely focused on inertial measurement. The app data processing is more complex that in the previous case, and the overall flow consists of Inputs (the Sensors), Functions (the data elaboration) and one Output (stream to BLE). The used function, the sensor fusion oriented to the calculation of the Euler angles (which describes the orientation of a rigid body in the 3D space), is widely described across ST literature (see for example UM2225, DT0060, DT0075). The source of the high accuracy of the described application are of course the sensors:

0690X000009jqbZQAQ.png

The below pictures are really very beautiful... and accurate 8) Have a look �?�

    This topic has been closed for replies.

    1 reply

    ST Employee
    September 30, 2019

    0690X000009jqjnQAA.png

    0690X000009jqkRQAQ.png