SensorTile.box #9: The Pro Mode - get a full control on all ST sensors
SensorTile.box tool is an open environment under almost all points of view. You can personalize the firmware, creating your own sensor package and you own neural network, and you can also customize the smartphone application interface, having a direct access in the source code.
At firmware level, you can program your ST.box in the best way for you. You can start a project from scratch (because the platform is included in the CubeMX code generator), or you can use the existing packages, which will be deeply described in the next posts:
- FP-SNS-STBOX1, the function pack dedicated to the Pro Mode of the SensorTile.box wireless multi sensor development kit;
- FP-AI-SENSING1, the function pack that enables for ultra-low power IoT node with artificial intelligence (AI) application based on audio and motion sensing;
- FP-SNS-ALLMEMS2, the classical function pack for ultra-low power IoT node with BLE connectivity, digital microphone, environmental and motion sensors.
At software level, the ST BLE Sensor application source code is open, and you can find in on Github.com --> here. Used in conjunction with a firmware compatible with the BlueST protocol, the ST BLE Sensor application allow the user to access to all the sensors data, to request and download algorithm licenses, and to update the firmware directly from a mobile device via the Bluetooth® Low Energy protocol.
So... let's start!