SensorTile.box Algobuilder User Button not working
Hi!
I am using the SensorTile.box together with Algobuilder. Since 2.6 there is the feature that pressing the user-button triggers data collection.
Unfortunately this does not seem to work with SensorTile.box. I am using the Example13_SensorTile.box_SDCard that comes along with Algobuilder. Setup is working fine. Everything works if I use Unicleo GUI. By pressing "Start" in the UI the blue led starts to blink and a file is generated on the SD Card.
But the problem is pressing the User Button just turns the led on (with low brightness level,) but no blinking. I can see in Unicleo that the "Start" and "Stop" buttons are enabled and disabled. Problem is that nothing is written on the SD Card.
I tried to display a graph at the same time:

By pressing the user button, Unicleo shows the data in the graph. However, the led is again not blinking and nothing is written on the SD card.
Is there anything that I have to change to make this work? I really would like to collect some data when not connected via USB to a PC running Unicleo.
Best wishes,
Dominik