Skip to main content
ST Employee
March 25, 2020
Question

SensorTile.box #collaterals: an insight into the Cloud feature of ST BLE Sensor application

  • March 25, 2020
  • 1 reply
  • 573 views

The STBLESensor application is not only the smartphone application for interfacing the SensorTile.box with the user and for setting the Mode 1 and Mode 2 examples via BLE, but it is also the graphical interface for a lot of other ST demo boards, reference designs and application platforms, such as the Bluecoin and Bluecoin2 kits, the Sensortile one and a few NUCLEO-like platforms.

Among the user-platform interfacing features, this application allows sending the sensor data to a cloud provider and requires a mobile phone with a working Internet connection (otherwise, it remains disabled).

The application supports the following platforms:

  • Generic MQTT;
  • Azure IOT Hub (Microsoft);
  • AWS IoT (Amazon);
  • Watson IoT platform (IBM).

For further details, please take a look at the user manual UM2499 (LINK)

    This topic has been closed for replies.

    1 reply

    ST Employee
    March 25, 2020

    Tipical STBLE Sensor Cloud screen

    0693W000000UiWkQAK.jpg