SensorTile.box does not work sometimes
Hello, I'm trying to measure a few things unsing the SensorTile.box. Sometimes everything works fine but then the SensorTile.box seems to be dead all of a sudden. When I then try to connect it to my Windows pc, the pc won't recognise it and my phone can't find it via bluetooth either. If I then disconnect the battery for a few seconds, reconnect it again and connect the SensorTile.box to the pc it starts charching and everthing works properly till it crashes again.
I don't think that this is a battery problem because when it's working it shows more than 3.3 V via bluetooth and I'm charging it whenever I'm not measuring. I haven't updated the firmware and just used the app to start and stop data logging. Then I transferred the measurement data to my pc with the USB-cable.