Skip to main content
Visitor II
October 5, 2023
Question

SensorTile.box PRO SWD not connect target!!!

  • October 5, 2023
  • 3 replies
  • 1624 views

Hi, I purchased the SensorTile.box PRO sensor, but I can't develop because it doesn't connect to the STLINK V2-1, in the datasheet it says:

1.jpg

I connect adapter STEVALMK1 (that was inside the kit) with STLINK V2-1

But I have the following error

2.jpg

 

 

the documentation is really bland

 

 
    This topic has been closed for replies.

    3 replies

    Technical Moderator
    October 6, 2023

    Hi @michelemancini2 ,

    May I ask you for some photo of the connections (STEVALMK1+STLink+board) and the version of STMcube programmer?

    Also, did you try to update the STLink drivers?

    Visitor II
    October 7, 2023

    If I use the latest STLink firmware, I use STLink of the "Nucleo F401RE". In the datasheet it says that it is possible to use stlink from the Nucleo dev board.
    This is the connection

     

    1.jpg2.jpg

    Graduate II
    October 7, 2023

    Cannot you see that the ST-LINK Utility is deprecated? Also update the ST-LINK firmware!

    Technical Moderator
    October 11, 2023

    Hi @michelemancini2 ,

    As said by @Piranha is correct. I suggest you an update of ST-LINK, driver update and an update of cubeprogrammer. Then disconnect and reconnect all.

    If this solves your problem, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.