SensorTile.box, unable to connect through the GATT interface on Windows
Hello,
Is there any reason which could explain I cannot connect to the sensor using GATT interface on Windows ?
The sensor often return, file not found, aborted or it is not able at all to connect to the sensor.
Application of ST in IOS works. Custom application with accelerometer has been pushed.
The only difference I have if I compare with another sensor which is working, it is the passcode.
Regards,