Skip to main content
Visitor II
November 22, 2020
Solved

SensorTile Dev Kit (STEVAL-STLKT01V1) - Not responding after a firmware update

  • November 22, 2020
  • 1 reply
  • 978 views

I just started using the SensorTile Dev Kit for one of our projects. As part of testing, I was trying to update the firmware using the ST BLE Sensor app but ran into problems. The firmware file was uploaded successfully but the board stopped responding. After waiting for a while, I tried the reset button but still no luck. 

I'm using the SensorTile mounted on the cradle expansion board in the kit. Is there a way to recover or reset this SensorTile? We have a ST-LINK/V2 available here but not any connectors that works with the cradle.

Is it possible to use the ST-LINK or another way to recover this SensorTile? Any suggestion that you can give is greatly appreciated. 

Thank you!

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @IVall.1​ ,

    I can suggest you to refer to this link, that explains you step-by-step the procedure for flashing a new firmware on the Sensortile platform.

    If you have a X-Nucleo you can use it (with the cable provided with the Sensortile), otherwise you should adapt the connector to the STLINK V2 (or just separate the wires connecting the pins point by point).

    -Eleon

    1 reply

    ST Employee
    November 24, 2020

    Hi @IVall.1​ ,

    I can suggest you to refer to this link, that explains you step-by-step the procedure for flashing a new firmware on the Sensortile platform.

    If you have a X-Nucleo you can use it (with the cable provided with the Sensortile), otherwise you should adapt the connector to the STLINK V2 (or just separate the wires connecting the pins point by point).

    -Eleon

    IVall.1Author
    Visitor II
    November 30, 2020

    Thank you very much! The link that you provided is very helpful. I should be able to flash a new firmware using these instructions.