SensorTile STLKT01V1 Where to get source code to pre-installed demo program?
For mechanical reasons we are using the Square SensorTile contained in the STEVAL-STLKT01V1 kit. This comes with demo software installed that shows off all of the features of the board. The demo advertises itself as AM1V330.
However, if we download the SDK V2.5.0 and build the BLE_SampleApp and program it into the Tile it advertises itself as STLB250 and is missing a lot of the functionality of the pre-programmed demo. It only has Temperature, Pressure, RSSI and a LED switch. My proof of concept demo needs the accelerometer support. Is the demo source available?