Skip to main content
Visitor II
October 3, 2018
Question

Solder-Bridge configurations for 4-microphone acquisition on the CCA02M1 module.

  • October 3, 2018
  • 0 replies
  • 520 views

Hello,

I am using an Nucleo - F401RE MCU, with the CCA02M1 module, and the STEVAL-MKI155V1 microphone coupon board and have encountered an issue with acquiring 4 audio channels.

Using the Acoustic Source Localisation program provided in the X-cube-MEMSMIC1 package, I can build the project, but when I debug, I encounter an Audio Error in the CCA02M1 driver, when it checks the SPI receive.

if(HAL_SPI_Receive_DMA(&hAudioInSPI, (uint8_t *)SPI_InternalBuffer, X_NUCLEO_CCA02M1_Handler.PdmBufferSize) != HAL_OK)
 {
 return AUDIO_ERROR;
 }
 }

Due to this, the only thing I can think the issue may be, is the solder bridge configuration. I followed the user manual configuration attached.

0690X000006C7XsQAK.png

I have triple checked the configurations, and checked continuity with a multi-meter, and there doesn't seem to be any issue with it, but its the only thing I can think of.

I can still upload the microphone streaming code, and am able to record audio with 2 microphones.

Thanks in advance for any help.

Damien

0690X000006C7YHQA0.png

    This topic has been closed for replies.