SPI connections from Nucleo-g070RB to STEVAL-MKI164V1/LIS2HH12 trouble reading device ID (WhoAmI)
I'm trying to get an accelerometer connected to my Nucleo-g070RB. I've got the STEVAL-MKI164V1 board with a LIS2HH12 on it.
The problem I have is I always get either zero of 0xFF when try to read the device ID (WhoAmI) which is not correct.
The 2 boards are wired up as:
+3.3V ------- Vdd
+3.3V ------- Vdd_IO
Ground ------ Ground
PA6 --------- JP2(22) SDO
PA7 --------- JP2(21) SDA/SDI/SDO
PA1 --------- JP2(20) SCL/SPC
PA4 --------- JP2(19) CS

From my .ioc file I've configured things as follows
Data Size : 8bits
First Bit: MSB First
CPOL: High
CPHA: 2 Edge
Also I've configured PA4 as a digital output to use for CS

I found another post in this forum indicating these settings are correct LIS2HH12 does not respond on SPI
Initially I thought that CPHA should have been on 1 Edge. With this setting change I get FF every time instead of the first few samples.
The GPIO settings from the .ioc file look like this


I've included the files lis2hh12_reg.c and lis2hh12_reg.h from the github repo STMicroelectronics/lis2hh12-pid
I used the examples in the github repo STMicroelectronics/STMems_Standard_C_drivers/lis2hh12_STdC/examples/lis2hh12_self_test.c as a guide for how to set things up.
The platform read and write functions look like (note that the HAL_Delay(1) in the platfrom_read is actually just something I added as a test but I had a version without the delay and it didn't seem to make any difference)
stmdev_ctx_t dev_ctx;
int32_t platform_write(void *handle, uint8_t Reg, const uint8_t *Bufp, uint16_t len){
HAL_StatusTypeDef result = 0;
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
result |= HAL_SPI_Transmit(handle, &Reg, 1, 1000);
result |= HAL_SPI_Transmit(handle, (uint8_t*) Bufp, len, 1000);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
return result;
}
int32_t platform_read(void *handle, uint8_t Reg, uint8_t *Bufp, uint16_t len){
HAL_StatusTypeDef result = 0;
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
HAL_Delay(1);
result |= HAL_SPI_Transmit(handle, &Reg, 1, 1000);
result |= HAL_SPI_Receive(handle, Bufp, len, 1000);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
return result;
}
Then in my main I've added
uint8_t whoamI;
dev_ctx.write_reg = platform_write;
dev_ctx.read_reg = platform_read;
dev_ctx.handle = &hspi1;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_Delay(1000);
//ReadRegister(WHO_AM_I,rxData);
lis2hh12_dev_id_get(&dev_ctx, &whoamI);
printf("%2X\n\r",whoamI);
}
/* USER CODE END 3 */
When I run this code I get output that looks like this in my serial log
FF
FF
0
0
0
0
0
0
0
I've tried a variety of different prescalers to slow down the baud rate but that has not helped.
I've also tried an alternate approach where instead of using the code from the lis2hh12-pid github page I do something like this instead. I tried a variety of permutations of this function with no luck.
HAL_StatusTypeDef ReadRegister(uint8_t addr, uint8_t *byte)
{
HAL_StatusTypeDef hal_status;
uint8_t tx_data[2];
uint8_t rx_data[2];
tx_data[0] = addr | 0x80; // read operation
tx_data[1] = 0; // dummy byte for response
rx_data[0] = 0;
rx_data[1] = 0;
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
HAL_Delay(1);
hal_status = HAL_SPI_Transmit(&hspi1, tx_data, 2, 1000);
hal_status = HAL_SPI_Receive(&hspi1, rx_data, 2, 1000);
HAL_Delay(1);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
if (hal_status == HAL_OK)
{
*byte = rx_data[1]; // response is in the second byte
printf("%2X,%2X\n\r",rx_data[0],rx_data[1]);
} else {
printf("hal_status is HAL_NG\n\r");
}
return hal_status;
}
I don't have a logic analyzer handy but I have tested my CS line with a multimeter and some test code to set that low and high on 1 second intervals and it seems to be working correctly.
I've tried putting in little delays as well as just tying CS to ground with no luck.
I've also tried a version where instead of using the lis2hh12_reg files from the github repo. I included the software component

for the LIS2DH12

And set up my platform read and writes the same as the code sample I provided. That did not produce different results.
I've also tried a version where I connect CS to PB0 and select Hardware NSS Output Signal

Which gives me SPI GPIO configuration that looks like this

In this case I removed the code from my platform read/write to pull CS low before communicating with it. When I did this I get 0xFF every time.
I've been using these documents as a reference DM00096789.pdf, STEVAL-MKI164V1 & Nucleo-64 boards
If anyone has any idea what I can do to get the SPI connection to the sensor working correctly I would greatly appreciate it.
Thank You