Question
Start-up state of L3GD20 and SPI bus
Posted on January 10, 2014 at 20:15
On power-up, does this gyroscope come up in operating, sleep, or power-down mode (i.e., when all SPI peripherals in my instrument are powered up by a common bus, how much is the gyro drawing?
The datasheet says that Vdd may be disconnected (powering off measurement functions) but if Vdd-IO is maintained the (SPI) bus ''is not blocked.'' I assume this means that SDO and SDI are not pulled low by the powered-down gyro. What is current drain from Vdd-IO when Vdd is off?I plan to use this gyro to measure slow (even < 1dps) rotation of an oceanographic drifter. Can you reassure a mere biologist that this is an appropriate device?Thanks!Tom WolcottProfessor Emeritus #gyroscopes