Question
State Machine and stack size ?
Dear Members,
I have a state machine but it seems that it stuck in one state,
Is it related with stack size ?
It's stuck on "case PULSE_IDLE" no matter the value of sensor_value,
The code :
switch(currentPulseDetectorState)
{
case PULSE_IDLE:
if(sensor_value >= PULSE_MIN_THRESHOLD) {
//printf("Sensor_value PULSE_IDLE %f \r\n",sensor_value);
currentPulseDetectorState = PULSE_TRACE_UP;
values_went_down = 0;
printf("PULSE IDLE\r\n");
return true;
}
break;
case PULSE_TRACE_UP:
printf("Sensor value PULSE_TRACE_UP %f\r\n",sensor_value);
if(sensor_value > prev_sensor_value)
{
printf("PULSE TRACE_UP\r\n");
currentBeat =HAL_GetTick();
lastBeatThreshold = sensor_value;
}
else
{
printf("Peak reached: ");
printf("%f \r\n",sensor_value);
printf(" ");
printf("%f \r\n",prev_sensor_value);
uint32_t beatDuration = currentBeat - lastBeat;
lastBeat = currentBeat;
float rawBPM=0;
if(beatDuration > 0)
rawBPM = 60000.0 / (float)beatDuration;
printf("RawBPM = %f\r\n",rawBPM);
//This method sometimes glitches, it's better to go through whole moving average everytime
//IT's a neat idea to optimize the amount of work for moving avg. but while placing, removing finger it can screw up
//valuesBPMSum -= valuesBPM[bpmIndex];
//valuesBPM[bpmIndex] = rawBPM;
//valuesBPMSum += valuesBPM[bpmIndex];
valuesBPM[bpmIndex] = rawBPM;
valuesBPMSum = 0;
for(int i=0; i<PULSE_BPM_SAMPLE_SIZE; i++)
{
valuesBPMSum += valuesBPM[i];
}
bpmIndex++;
bpmIndex = bpmIndex % PULSE_BPM_SAMPLE_SIZE;
if(valuesBPMCount < PULSE_BPM_SAMPLE_SIZE)
valuesBPMCount++;
currentBPM = valuesBPMSum / valuesBPMCount;
printf("AVg. BPM: ");
printf("%f",currentBPM);
currentPulseDetectorState = PULSE_TRACE_DOWN;
return true;
}
break;
case PULSE_TRACE_DOWN:
if(sensor_value < prev_sensor_value)
{
values_went_down++;
}
if(sensor_value < PULSE_MIN_THRESHOLD)
{
currentPulseDetectorState = PULSE_IDLE;
}
break;
}
prev_sensor_value = sensor_value;Any clues on solving it ? thanks