Skip to main content
Visitor II
July 28, 2025
Solved

STEVAL-FCU001V2

  • July 28, 2025
  • 1 reply
  • 408 views

I'm new to the STEVAL-DRONE2 kit and would like to ask: Given that the STEVAL-FCU001V2 flight control unit includes basic sensors like the IMU and barometer, can it support the integration of additional external sensors, such as GPS modules, magnetometers, optical flow, LiDAR, or ultrasonic sensors, through STM32? And are there any specific hardware or firmware considerations I should be aware of when adding these to the system?

    This topic has been closed for replies.
    Best answer by KnarfB

    The STEVAL-FCU001V2 has some spare interfaces which you could use if you change the firmware accordingly. The STEVAL-DRONE2 is really a mini drone, I consider it more a proof of concept. So it will not be able to carry any but the lightest sensors. 

    hth

    KnarfB

    1 reply

    KnarfBAnswer
    Super User
    July 28, 2025

    The STEVAL-FCU001V2 has some spare interfaces which you could use if you change the firmware accordingly. The STEVAL-DRONE2 is really a mini drone, I consider it more a proof of concept. So it will not be able to carry any but the lightest sensors. 

    hth

    KnarfB

    sani-kAuthor
    Visitor II
    July 29, 2025

    Thank you very much