STEVAL-MK141V2 (HTS221) temp/RH sensor
Hi, I got the reference board of STEVAL-MKI141V2 that has HTS221 temperature and humidity sensor.
#1
I read out the calibration registers by the manual of https://www.st.com/resource/en/technical_note/tn1218-interpreting-humidity-and-temperature-readings-in-the-hts221-digital-humidity-sensor-stmicroelectronics.pdf and the result is following.
H0_rH_X2 (30) = 3A, H1_rH_x2 (31) = 87, T0_degC_x8 (32) = A7, T1_degC_x8 (33) = 16
T2/T0 msb (35) = 4
H0_T0_OUT (36,37) = FFFB, H1_T0_OUT (3A,3B) = D6E4
T0_OUT (3C, 3D) = FFFF, T1_OUT (3E, 3F) = 0310
So the registers value of H0_T0_OUT, H1_T0_OUT also T0_OUT value are minus, is that normal?
#2
It seems the temperature and humidity can be calucuated from there registers. 25.5 degree and 57% RH
but humidity is more 10% higher than other sensors. The accuracy is out of specification value +/- 3.5%.
#3
I want to check the device that using HTS221 sensor, Could you let me know brand and model name if someone knows any products those using HTS221?
Thank you for reading