steval-mki109d with steval-mki245KA standalone logging
Hello,
I was wondering if it is possible to set the steval-mki109d with steval-mki245KA to standalone.
I would like to test the ISM330BX what is happening when rotating. Thus I have set up a kit with a battery pack and I can start up the measurement with MEMS studio 2.0. When I just pull out the USB-C connector, I think everything will go on (LEDs keep doing the same thing as when i turned the mems on in MEMS studio). But when I reconnect to MEMS studio the ISM330BX will have to be configured again. Meaning I cannot check the final values after rotating.
Is there any way to for example log all the data to a SD card without writing all the code by myself? Or any other way to read out the final value without the processor/MEMS resetting?
Thanks!