Question
STEVAL-MKI109V2 with STEVAL-MKI142V1 - I2C mode
Posted on July 29, 2015 at 17:05
All:
I have procurred a STEVAL-MKI109V2 and plug-in board STEVAL-MKI142V1 (LPS25H). When I bring up the UNICO ''Cross-platform User Interface for MEMS demonstration kits'', I am able to see that the device is operating, and it has good values. However, can the interface be changed from the default SPI to run as I2C?I would like to do this to evaluate a target board that has been made up with an I2C interface.I realize that I2C may not be an option for the demo, but is it an option?If so, how do I change the UNICO settings to use the I2C option?Regards,Todd Anderson #unico