Skip to main content
Visitor II
July 17, 2019
Question

STEVAL-MKI159V1 with STEVAL-MKI109V3 - Unico does not allow magnetometer configuration?

  • July 17, 2019
  • 1 reply
  • 666 views

I have bought these two evaluation boards. The accelerometer and gyroscope work fine. The magnetometer settings in Unico do not change the magnetometer registers. Reading magnetometer registers returns ff at all times. If I have a logic grabber connected to the I/O pins of the sensor the board then Unico does not start properly (complains WHO_AM_I is wrong).

I cannot read anything out of the magnetometer. Is this a known issue?

    This topic has been closed for replies.

    1 reply

    Visitor II
    July 17, 2019

    Minor update, results identical on Windows 10 and Ubuntu 18.04. Using Unico 9.0.0 and ProfiMEMSTool 3.2.6, up to date as of yesterday.