STEVAL-MKI192V1 (LPS22HH) - 50% failure on delivery
Hello
I ordered 10 samples of the LPS22HH pressure sensor evaluation board (STEVAL-MKI192V1). Upon receipt, I noticed that each board was packaged in a cardboard box but without an anti-static bag.
I then began taking measurements by varying the pressure inside a test chamber. Out of the 10 samples, only 5 function correctly and measure the expected pressure, while the remaining 5 consistently read only 1 bar.
Could this be due to the high sensitivity of the board and the sensor itself, or could it be a delivery issue? I find this particularly concerning as I ordered from three different distributors and encountered the same issue. This leads me to wonder if the sensor is particularly fragile. Could you provide any insights on this?
thanks