STEVAL-MKI197V1: Pedometer Regression tool not working in offline mode
Hello,
I am working with STEVAL-MKI197V1 to evaluate the steps detected by the pedometer.
By looking at the documentation, I found out that the pedometer can be better configured by using the UNICO GUI.
At the moment, I do not have the STEVAL-MKI109V3 motherboard, but I read that the Regression Tool can be used offline with custom data written in a specific format.
Therefore, I tried to use the regression tool with a simple txt file ('test_steps50.txt') containing the following data:
A_X [mg] A_Y [mg] A_Z [mg]
251 900 -119
259 907 -132
271 907 -145
276 904 -162
280 915 -166
263 908 -163
260 882 -171
225 869 -165
224 863 -181
228 860 -210
*Data are spaced with tabsIf I choose the folder containing this file and the output directory, after running the tool I do not get any configuration file (.ucf). The only file I get is the 'regression_tool.config' file in a different path with respect to the output directory defined in the UNICO GUI. However, this file is just telling me some data about the regression process.
I tried with different data logs (also those found in ST github repositories in which the files contain both the accelerations and gyroscope data) but nothing changed.
I am currently using a MacOS Monterey with chip Apple M1 Pro
Thanks in advance for your help