STEVAL-MKI208V1K (IIS3DWB) and Nucleo-WB55RG : SPI not working, Pin CS at 3.3v?
Hi,
(Since i am not a native speaker i apologize in advance for any mistake i would make.)
I am curently working on a project that require an acelerometer.
For my tests, i am working with a NUCLEO-WB55RG and an eval board STEVAL-MKI208V1K. They are connected together through SPI1 like follows:
Nucleo ---> Eval Board
(SCK) PA5 [D13] ---> SCL
(MISO) PA6 [D12] ---> SDA
(MOSI) PA7 [D11] ---> SDO
(CS) GND ---> CS
When i check the levels i can see that the chip select is somehow at 3.3V !
Is there a register to parameter or something to do to specify that i don't want to use the chip in I2C but in SPI (and so put the CS to ground level).
Thank you in advance ,
Noé.