Skip to main content
Explorer
June 20, 2025
Question

[STEVAL-PROTEUS1] Bootloader hangs at SHCI_C2_BLE_Init after SystemReset from application

  • June 20, 2025
  • 1 reply
  • 308 views

Hello ST team,

I’m currently developing on the STEVAL-PROTEUS1 platform and encountered an issue when transitioning from the application firmware to the bootloader.

Specifically, after executing a jump from the application to the bootloader (located at 0x08000000), the bootloader hangs during CPU2 initialization. It gets stuck at the following function call:

SHCI_C2_BLE_Init(&ble_init_cmd_packet);

This only occurs when jumping from the application. When powering on the board directly into the bootloader, everything works as expected, and BLE initialization succeeds.

I have ensured that:

  • CPU2 is not held in reset by the application before the jump.

  • The jump procedure clears necessary registers (SCB->VTOR, stack pointer, etc.).

Despite this, SHCI_C2_BLE_Init() does not return or proceed further.

Has anyone experienced similar behavior on the STEVAL-PROTEUS1 or other STM32WB-based boards? Are there additional steps required to properly re-initialize CPU2 when switching from application to bootloader?

Any suggestions or guidance would be greatly appreciated.
Thanks in advance!

Best regards,

    This topic has been closed for replies.

    1 reply

    hanyangAuthor
    Explorer
    June 20, 2025

    As a follow-up to my previous question regarding SHCI_C2_BLE_Init() hanging in the bootloader after jumping from the application — I would like to confirm one key detail related to OTA updates.

    If I want to implement BLE-based OTA firmware upgrade (e.g., using ST’s STM32CubeProgrammer or a custom mobile app), does the bootloader need to reinitialize the BLE stack and expose a BLE service again, after jumping from the application?

    Or is it possible to perform OTA upgrades entirely within the application, without jumping to the bootloader?

    I understand that the reference bootloader examples usually reinitialize BLE and expose specific characteristics, but I want to know whether that's strictly required — or whether I can build OTA functionality directly into the application and skip bootloader involvement entirely.

    Thank you for your clarification.