STEVAL-Proteus1 many issues in demo App
I tried all 3 available demos: default, FP-AI and Datalogger.
At last I flashed the original default demo back. All tests are done USB-powered or with LiPo.
Establishing a BLE connection with iPhone works in 10% of the cases.
Using an Android smartphone is more successfully.
All issues found:
- No plot data of gyro and accelerometer, but FFT and Board Pred Maintenance worked.
- In plot data the axes and 3 colored lines were shown at zero level, but no lines are changing (regardless autoscale setting).
- FFT shows sometimes lines horizontically like in plot data, no vertical bars and frozen.
- Or no sensor data at all, but I can turn on/off LED (very nice)
- Or plot data does not scroll, lines were drawn back and forth
- BLE interrupted on iPhone
Version FW: WB5MMG_STSW-PROTEUS_1.1.0 (from STEVAL-Proteus1 package) BLE-CbM
Having the latest BLE stack from Github (V1.20.0 build 2), because one ST employee noticed an older one (V1.19.0) in the current STEVAL-Proteus1 package.
I tried to show the demo to a customer in their factory and it ended not well.
Do I have to wait for STEVAL-Proteus 1.2.0 ?
Best regards