STEVAL-SMARTAG humidity sensor readout problem
I have flashed the example code from the function pack on 2 STEVAL-SMARTAG modules using a Nucleo STLink. After flashing, I get very different (incorrect) values from the humidity sensor (31% whereas the original sensor, as purchased, read the correct value of 48%). The temperature sensor is still fine.
The code I used is:
en.fp-sns-smartag1\STM32CubeFunctionPack_SMARTAG1_V2.0.0\Projects\STEVAL-SMARTAG1\Examples\SmarTag1\MDK-ARM\Project.uvprojx
I use an iPhone to read the sensor via NFC. Does anyone know what could be the problem?
Is the code that is supplied on the SMARTAG module different from the example code?