Skip to main content
Visitor II
February 7, 2021
Solved

STEVAL-STWINKT1 vs STEVAL-STWIN KT1B

  • February 7, 2021
  • 2 replies
  • 1298 views

We purchased late in 2020 an STEVAL-STWINKT1.

Just learnt that this board has been deprecated and the  STEVAL-STWIN KT1B is instead the recommended reference design

Could you please let us know:

  • if we have to stop using the STEVAL-STWINKT1
  • if get it replaced by the STEVAL-STWINKT1B

BR

DS

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi DS @dsamm​ ,

    In general, you can indifferently use the STEVAL-STWINKT1 platform or the STEVAL-STWIN KT1B one, except in the case you want to use the new features, that are summarized as follow:

    • STM32L4+ “U�? part number to enable MCD locking mechanism for 3rd party libraries (as in all mcd Nucleo/Disco/EVAL board)
    • STSAFE-A110: soldered directly on the board
    • IMP23ABSU: Ultrasound industrial-grade analog MEMS microphone --> but this is very similar to the MP23ABS1 in most cases
    • BlueNRG-M2SA: (new) BlueNRG-2 BLE module
    • New plastic to satisfy anti inflammability requirements (blue)

    At the moment, the only software designed to run exclusively on the new STEVAL-STWIN KT1B is the FP-AI-NANOEDG1, that uses the locking mechanism for 3rd party libraries.

    So, if you are using the platform regardless the hardware differences, you can safely use the STEVAL-STWINKT1.

    In case this answer was helpful for you, please select it as "best".

    -Eleon

    2 replies

    ST Employee
    February 8, 2021

    Hi DS @dsamm​ ,

    In general, you can indifferently use the STEVAL-STWINKT1 platform or the STEVAL-STWIN KT1B one, except in the case you want to use the new features, that are summarized as follow:

    • STM32L4+ “U�? part number to enable MCD locking mechanism for 3rd party libraries (as in all mcd Nucleo/Disco/EVAL board)
    • STSAFE-A110: soldered directly on the board
    • IMP23ABSU: Ultrasound industrial-grade analog MEMS microphone --> but this is very similar to the MP23ABS1 in most cases
    • BlueNRG-M2SA: (new) BlueNRG-2 BLE module
    • New plastic to satisfy anti inflammability requirements (blue)

    At the moment, the only software designed to run exclusively on the new STEVAL-STWIN KT1B is the FP-AI-NANOEDG1, that uses the locking mechanism for 3rd party libraries.

    So, if you are using the platform regardless the hardware differences, you can safely use the STEVAL-STWINKT1.

    In case this answer was helpful for you, please select it as "best".

    -Eleon

    dsammAuthor
    Visitor II
    February 8, 2021

    thanks!

    -daniele