Steval-STWINKT1B - Where is all the power going?
On the STEVAL-STWINKT1B board, and using the HSDatalog firmware, it uses about 60mA in idle state. I have disconnected the sensors, and the uC, and turned off the SD card power lines, but it's still at around 2mA. Does anyone know where this power is going? Ideally, I want to create an application for the board when it wakes up for 1 minute in every hour, logs the data to the SD card, and then goes into a nearly dormant low power state to preserve the battery.