Skip to main content
Visitor II
December 9, 2025
Question

STHS34PF80 – Data remains constant, TOBJECT = -48

  • December 9, 2025
  • 1 reply
  • 73 views

Hello,
I am trying to get the STHS34PF80 sensor working on an STM32L0 platform via I²C. My initialization sequence is as follows:

  1. Algorithm reset according to AN5867:
CTRL2 (0x21) = 0x10 // FUNC_CFG_ACCESS = 1
PAGE_RW (0x11) = 0x40 // FUNC_CFG_WRITE = 1
FUNC_CFG_ADDR (0x08) = 0x2A
FUNC_CFG_DATA (0x09) = 0x01
PAGE_RW (0x11) = 0x00
CTRL2 (0x21) = 0x00
  1. Interrupt configuration:
    CTRL3 (0x22) = 0x05

  2. AVG_TRIM:
    0x10 = 0x01

  3. Continuous mode:
    CTRL1 (0x20) = 0x15 (BDU=1, ODR=4 Hz according to datasheet)

After this, I wait for EXTI interrupt (DRDY). On interrupt, I read:

  • STATUS (0x23)
  • TOBJECT_L/H (0x26/0x27) and etc.
  • FUNC_STATUS (0x25)

Problem:

  • The TOBJECT value remains constant (-48), even when I place a hand or heat source in front of the sensor.
  • Presence/motion flags in FUNC_STATUS almost never change. Occasionally, I see a value of 1, but very rarely, even when moving a hand or breathing near the sensor.
  • See attached screenshot of current data from the terminal.

Questions:

  • Is my initialization sequence correct?
  • What could cause TOBJECT to stay constant?
  • Are there recommended threshold and AVG settings for reliable detection?

Thanks for any tips or reference to a working example.

    This topic has been closed for replies.

    1 reply

    ST Employee
    December 24, 2025

    Hi @los_trpaslikos ,

    Are you using STM32L0 platform together with a custom PCB with STHS34PF80? Can you please give us more details on you HW setup? Did you find out this issue only on one part?