Skip to main content
Explorer
April 25, 2024
Question

STHS34PF80 proximity application

  • April 25, 2024
  • 1 reply
  • 1347 views

Hi everyone,

I'm developing a tamper detection circuit for a meter enclosure. I'm considering the STHS34PF80 infrared proximity sensor, but I'm struggling to find reference materials or application notes specifically related to tamper detection using this sensor.

My goal is to use the sensor as an interrupt generator, similar to a switch. When someone opens the enclosure lid, the sensor should detect the change in proximity and trigger an interrupt signal to the microcontroller, indicating tampering.

Can anyone recommend reference materials or alternative sensor options suitable for tamper detection in this application?

Thanks.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    April 29, 2024

    Hi @dhruvit ,

    We don't have specific reference material for this application but, as far as I can tell from your post, you can use a presence library to detect if someone is in proximity.

    You can tune the algorithm following the AN.

     

    For the presence detection library, you can refer to X-CUBE-MEMS1

    https://www.st.com/en/embedded-software/x-cube-mems1.html?icmp=tt33855_gl_lnkon_jul2023

     

    Here an example for presence detection:

    https://github.com/STMicroelectronics/X-CUBE-MEMS1/tree/main/Projects/NUCLEO-F401RE/Applications/CUSTOM/PresenceDetection_STHS34PF80

    Visitor II
    June 11, 2025

    Is it possible to get source code to the library ? We are using different type of MCU in the project. Under NDA or something. Currently we are facing very unstable presence detection based on examples from internet and consider resign using STHS if we don't overlap problems. 

    -sensor is saturated in some case

    -unstable presence detection after condition are changed (  internal temperature ) besides  we update current reference ambient temperature.