STM32CubeMX (5.2.1.) + X-CUBE-BLE1 (4.4.0) code generated SensorDemoBLESensor failes to init properly.
I generate the code for my B-L475E-IOT01A board. That board works well, e.g. with HeartRate sample from STM32Cube_FW_L4_V1.14.0. But, I want to generate BLE code using STM32CubeMX. I choose my board type, check Wireless BlueNRG-MS and Wireless Application under Additional Software. I choose SensorDemoBLESensor, HCI_TL Basic and HCI_TL_INTERFACE User Board and generate the code for SW4STM32.
When I build, I get errors compiling b_l475e_iot01a_bus.c because of undefined symbols INTERNAL_SPI3_..._Pin, so I manually include main.h. (Why is this needed?)
Now, build completes, but the debugger gets stuck forever during SPI reset:
Thread #1 (Suspended : Signal : SIGINT:Interrupt)
SPI_EndRxTxTransaction() at stm32l4xx_hal_spi.c:3.941 0x80027d0
HAL_SPI_TransmitReceive() at stm32l4xx_hal_spi.c:1.475 0x8002b62
BSP_SPI3_SendRecv() at b_l475e_iot01a_bus.c:192 0x8004a2e
HCI_TL_SPI_Receive() at hci_tl_interface.c:123 0x80050ba
hci_notify_asynch_evt() at hci_tl.c:359 0x8003e94
hci_tl_lowlevel_isr() at hci_tl_interface.c:282 0x80051f6
HAL_EXTI_IRQHandler() at stm32l4xx_hal_exti.c:528 0x8000ec4
EXTI9_5_IRQHandler() at stm32l4xx_it.c:209 0x8005b6a
<signal handler called>() at 0xfffffff9
HAL_Delay() at stm32l4xx_hal.c:405 0x8000c4a
HCI_TL_SPI_Reset() at hci_tl_interface.c:98 0x800507a
hci_init() at hci_tl.c:178 0x8003ca8
MX_BlueNRG_MS_Init() at app_x-cube-ble1.c:131 0x8004854
main() at main.c:111 0x80056fe
Any ideas what went wrong and how to recover? Are there working eamples, tutorials?